Nouvelles de la société
EASA Convention 2017 | June 25-27, Tampa
The annual EASA conference & convention is quickly approaching in Tampa, Florida. If your attending this year, be sure and stop by booth #501 to visit your friends from Baldor! We have an exciting lineup for EASA this year and would like nothing more than to share with you. This year’s convention runs from June 25-27 at the Tampa Convention Center.
“As a supporter and exhibitor at EASA for more than 30 years, we value our relationship with the organization and its members. They are our service arm for electrical products.” noted Randy Colip, Executive Vice President Sales. “Each year, we look forward to attending the annual convention to catch up with old friendships and make new ones.”
In the booth this year, we’ll showcase a number of stock and custom products including:
RPM XE: A product line built with a caged permanent magnet rotor. The RPM XE is a hybrid motor platform that can operate across the line or on adjustable frequency power. When operated across the line the platform offers up to 4 levels above NEMA Premium® efficiency or when paired with a drive meets NEMA Premium efficiency. The standard NEMA frame design allows drop-in replacement for traditional NEMA motors.
Farm Duty: Designed and built with reliability at the forefront. Farm duty motors are put to the test every single day in some of the most rugged and harsh environments. Most three phase designs incorporate extra sealing around the shaft output and sealed bearings. The entire farm duty line is finished with a heavy duty epoxy paint to protect the motor from outdoor elements.
Crusher Duty: Engineered for the demands of the aggregate industry; the crusher duty platform offers high torque characteristics and superior reliability. Enclosures are rated for IP55 to keep dust, debris, and moisture out of the rotating and electrical assemblies. All ratings offer NEMA Premium efficiency.
RPM PD DC Motors: An optimized armature design allows for full power and increased torque across a wide speed range, while maintenance is minimized with enhanced brushes and monitoring devices.
Customer Appreciation Reception
We invite you to join us for a night of fun, food & entertainment as we say thanks for your partnership on Monday, June 26th at the Marriot Waterside Grand ballroom. The customer appreciation reception starts at 6:00PM and runs through 10:00PM. There will be games and activities for all ages and giveaways throughout the night! View your invitation HERE.