Company News
Join Baldor at EASA 2015
Baldor Electric Company will be attending the 2015 EASA convention and meeting in San Antonio, Texas June 14th through June 16th, 2015. As you walk the show, be sure to stop by booth #503 to visit with your friends from Baldor or to view some of our newest products available.
On display will be the Baldor-Reliance® Crusher duty motor platform which is available from stock in ratings of 5 - 350 Horsepower. Crusher duty motors meet Premium Efficiency energy standards and is complaint with the Integral Horsepower Rule, which goes into effect June 1, 2016. Performance of the new crusher duty line has been enhanced across the entire platform to provide greater breakdown and locked rotor torque values.
Baldor’s Large AC GPM motor platform will also be featured at the show. Available from stock in ratings of 250 – 1000 Horsepower in low voltage and medium voltage configurations. The Large AC GPM motor platform is also available in custom ratings of 250 – 1,500 Horsepower, also in low or medium voltage configurations.
ABB low voltage IEC motors will also be on display in the booth. Available in standard IEC frame designs, the process performance platform is available from stock in ratings of .16 – 125 Horsepower. Not limited to stock inventory, Baldor also offers a large variety of custom ABB IEC designs. Stop by the booth and ask about the complete line of ABB low voltage IEC motors from Baldor.
We also invite you to a customer appreciation event held Monday, June 15 in the Lone Star Ballroom on the 2nd Floor in the Grand Hyatt Hotel in San Antonio. The event runs from 6:00 PM – 11:00 PM. Come enjoy food, refreshments, and activities for all ages as we say Thank-You!
See You at EASA!