The Baldor Motor line is being upgraded to meet the energy efficiency requirements of the Energy Independence and Security Act of 2007 (“EISA”). Under EISA, all general purpose motors, from 1 to 200 horsepower, manufactured in the United States after December 19, 2010, must meet higher efficiency levels.
Baldor will offer customers two broad lines of energy-efficient motors in response the EISA:
- Compliance for General-purpose Subtype I motors will be by our Super-E family of motors that meet or exceed NEMA Premium® efficiency levels of NEMA MG1, table 12-12.
- The efficiency for 1-200 HP Subtype II motors and the 201-500 HP motors will be met by Baldor’s Standard-E motors; providing efficiency levels compliant with the requirements. Efficiency levels will be adjusted on some motors to meet EISA levels of NEMA MG1, table 12-11. Super-E NEMA Premium® efficient motors are available for these ratings that exceed EISA requirements for companies wishing to save on electrical costs.
The first to announce a plan to upgrade an existing line of standard motors to meet EPAct requirements, Baldor’s effort encompasses over 2,000 stock motor ratings.