Company News
New And Upgraded Dodge Sleevoil Components
Dodge Sleevoil hydrodynamic bearings are high performance products with a long history of use in industrial fan applications dating back to the 1930’s. Today, Sleevoil bearings are widely specified for industrial fans when uptime, reliability, and ease of maintenance is a must.
Sleevoil bearings are commonly found in the power generation, cement, pulp, paper, petrochemical, and steel industries. Customers in these industries rely on the superior performance of the bearing and its unique internal cooling options to keep their plant running in the most extreme conditions.
To further enhance the existing Sleevoil product line, Dodge is launching several new Sleevoil bearing components. These components can be utilized on existing Sleevoil installations or ordered with new Sleevoil pillow blocks and liners. The Dodge OLF and Cool Lube circulating oil systems have also been redesigned and offer new features and performance enhancements.