English
English
français (Canada)
Go

Company News

Turbomachinery and Pump Symposia

We are headed to Houston, Texas for the 45th Turbomachinery & 32nd Pump Symposia, September 12-15 and invite you to stop by the booth (#3141) to chat with industry experts from Baldor. Baldor will be showcasing a complete offering designed specifically for the pumping industry including motor and mechanical power transmission products.

Also on display is the new variety of Baldor-Reliance® motors including Above NEMA Vertical P-Base motors which meet standard NEMA specified P-Base dimensions for vertical pump applications. The platform features a grease lubricated ball bearing on the drive end with a thrust bearing on the upper (non-drive end) as standard. Oil lubrication and different bearing arrangements are optional features if the application is subject to heavy loading.

Stop by and learn how the new Baldor-Dodge Raptor coupling can decrease total cost of ownership and extend driven equipment life. Also, on display will be Baldor-Dodge Gear Reducers and mounted bearings used in the pumping industry.

See you in Houston!

Turbomachinery and Pump Symposia