Baldor Electric Company
Baldor
  Product Quick Search
Baldor
Our job is making yours easier. Worldwide.
HomeLocate DistributorContact UsSite Map
blank.gif
Products Support News/Events About Baldor Investor Relations


Press Releases
<< Return to list

March 29, 2006

Ethernet Motion Control Technology Catalyzes Breakthrough In Tube Bending Productivitiy

Fort Smith, AR, February 22, 2006 --- Ethernet-compatible servo motor drives are catalyzing a breakthrough in the performance of tube bending machinery - allowing multi-stage bending operations to take place in parallel, while also reducing the electrical bill of materials and machine footprint. The technology is installed on Unison's new machine, Breeze Uniflex, which provides modular multi-stage bending with automatic feeding, positioning and clamping to progress tube components through the process. The real-time motion and machine control hardware and software are provided by motion control technology from Baldor Electric (NYSE:BEZ) utilizing the deterministic Ethernet Powerlink networking protocol.

Each bend head is powered by a servo motor axis and drive. A single machine controller manages the complete real-time multi-stage bending process, along with numerous other feed and carriage axes. In the first production version of Breeze Uniflex, a machine Unison configured to produce condenser tubes for diesel engines, the controller manages a total of 15 motion axes as well as numerous I/O channels. On this application, tubing components progress automatically through four separate bending stages, with operations at each stage happening simultaneously.

The parallel processing multiplies productivity compared with the more typical sequential operation of a multi-head bender. Unison has also managed to reduce the size of the electrical control cabinet dramatically, by an estimated two thirds. This benefit was a combined result of much simpler wiring, and the ability of the machine controller - Baldor's NextMove(tm) e100 - to manage and synchronize all the motion axes and I/O required via the high-bandwidth (100Mbits/second) Ethernet network.

The centralized machine controller has comprehensive real-time control of each drive, allowing it to deterministically control parameters such as motor torque and speed, as tube components move through the machine. Such control would not have been possible with the motion architecture Unison employed on previous machines, which was based on standard servo drive amplifiers managed by a standard Windows PC. The performance of the Windows PC controller, and the basic analog control over servo motor characteristics, would simply not have supported either such sophisticated or fast operation without additional hardware and real-time extensions to the operating system.

The machine's simpler architecture, with its single Ethernet-based controller, also reduced software complexity. In fact, Unison managed to get a prototype version of the control program working within just one week of receiving the machine control software - Baldor's Mint programming language.

Programming speed was aided by the Mint software's built-in multi-tasking kernel, which allowed Unison's development team to divide the real-time control program into a number of discrete software modules. Programming the core bending control program was further simplified by using a single bend task throughout the machine, of which there can be several instances. The instances all run concurrently, providing simultaneous control however many bend stations are required; the first instance of the machine has four, but adding a further station would simply require the generation of code for another axis.

Mint's keyword programming structure, with high-level commands for motion operations, then provided a fast means of developing the motion tasks.

Operation of the machine is set up via a customized variant of Unison's existing human-machine interface (HMI) package - based on Visual BASIC - which interfaces to the NextMove machine controller via ActiveX calls. Mint's support for ActiveX also simplified this aspect of the programming. For example, on a previous Unison machine one element of the Visual BASIC front end required several hundred lines of code to manage the complex communication routines. This was reduced to just 25 lines on Breeze Uniflex, by simply referencing the ActiveX control provided.

"Baldor's Ethernet Powerlink technology provides such a leap in motion control performance that it makes this new multi-stage bending machine feasible," says Mike Kay, the Unison engineer responsible for the control system. "The machine operates at several times the productivity that would previously have been possible, and in a space that's probably half the size of the last generation."

In total there are 15 brushless servo motor axes on Unison's first machine, each controlled by one of Baldor's single-axis MicroFlex e100 drives. Four axes perform bending operations on the tube components. The remaining eleven feed, rotate and clamp tubing components. In addition to these major hardware elements, a number of I/O devices are controlled via the network, including an absolute encoder for automatic bend angle verification on each bend axis. For cost effectiveness, and to maintain the machine's modular architecture, many of the I/O components are connected locally to the controller using the CANopen fieldbus, an architectural possibility opened up by the decision of the Ethernet Powerlink standards body group to use CANopen device profiles, and the availability of a CANopen port on the Baldor drives.

Unison pioneered the use of electrical actuation technology for tube and pipe bending in the mid 1990s - delivering machines that operate on a small fraction of the energy used by traditional hydraulic benders, along with other benefits including quieter operation and drift-free accuracy. This latest machine re-emphasizes the technological lead of all-electric benders, multiplying productivity levels.

"The benefits of all-electric tube bending machinery are now strongly established, and the technology is taking a substantial slice of the market," notes Unison's Managing Director, Alan Pickering. "We believe all-electric technology now accounts for a fifth of the high-end tube bending market - which is around ten times the share of five years ago - and we expect market share to double again in the next five years."

Unison's latest machine extends the benefits of all-electric tube bending to the multi-head, high-throughput market, opening up major high volume manufacturing applications for the technology. Following the first installation of Breeze Uniflex at a major automotive manufacturer, Unison expects the higher levels of throughput that are now achievable to appeal to manufacturers of tubing components such as brake and power steering piping, and car seats.

Among the benefits offered by all-electric architecture are far better repeatability than a hydraulic machine, and automatic tooling set-up - because once a part has been produced successfully all the set-up data can be stored and recalled without any need for mechanical adjustments.

More efficient power utilization means that machines operate at probably 10-20% of the power consumption of a comparable hydraulic bender. There are additionally no large start-up inrush currents to contend with.

Quieter operation also results from the use of servo technology: Unison's new machine operates at around 55-60 dB normally - broadly equivalent to the noise levels in an office. This contrasts with perhaps 80-85 dB for a typical hydraulic bender with its larger power pack.

For further information please contact:

Reader contact:

Baldor Electric Company, P.O. Box 2400, Fort Smith, AR 72903, USA t: 479 646 4711; f: 479 648 5792; e: sales.us@baldor.com; www.baldor.com

Editorial contacts: Baldor: Charlie Hubbard, t: 479 646 4711: chubbard@baldor.com

Unison: Alan Pickering, Unison Ltd, Olympian Trading Estate, Cayton Low Road, Eastfield, Scarborough YO11 3BT, UK. t: +44 1723 582868; f: +44 1723 582379; e: enquiries@unisonltd.com; w: www.unisonltd.com

NextMove is a trademark of Baldor. Any other trade marks used are recognized and are the property of their respective owners.