Looking for old site? Looking for old site?

Looking for our old site?

We officially launched our new site on March 8, 2015.  There are many new features and we trust you’ll like the new site once you have a chance to explore all it can offer you.

While we hope our old sites served you well, unfortunately they are showing their age and we will be retiring them soon.  However, if you’re in a super big hurry and don’t have time to learn the new site, you can get to the old sites below for a limited time.

Old Sites
 www.baldor.com www.dodgept.com
 www.reliance.com www.dodge-reliance.com
Go

BE$T Energy Savings Software

The BE$T Baldor Energy Savings Tool is a software program that compares the efficiency and annual electricity usage of your existing motors. The program then calculates the annual potential savings. The program provides an estimated payback calculation and suggested replacement motor to make upgrades easier.

BE$T Baldor Energy Savings Tool Features

The BE$T Baldor Energy Savings Tool has several innovative features to facilitate data entry, storage and retrieval plus report writing capabilities.

  • Accepts data entry two ways, keyboard input or import of a project via Microsoft Excel.
  • Built in report writer for simple summary and detailed reports. An export feature provides complete access to the project’s data. Thus providing the data necessary to design custom reports.
  • Internet updates of the program code and data files to maintain accuracy.
  • Also currency conversion, project level energy costing, a motor management feature, estimated rewind costs and motor nameplate data.
  • New motor applications
  • Added Australian motors to the program
  • Added the ability to enter custom motors to the project file
  • Added the ability to select a motor from the available motor list
  • Updated the net pricing function
  • A custom printed report is now available
  • A customer logo can be easily added to the program
  • a potential CO2 saved report based on the project kWH saved
  • Can now import Excel 2007 .xlsx file types

System Requirement

The computer system must have one of the following operating systems: Windows 98, ME, NT 4.0, Windows 2000, or XP and Windows Vista.

Optional Requirements

Excel 97 or above recommended. To install, please RUN the file after downloading and respond to all screen prompts.

Screenshots

Single Motor View

BE$T Instant Cost Calculation View

Instant Cost Calulation

BE$T Single Motor View

CUSTOMER ACKNOWLEDGES AND AGREES THAT FOR ABB SOFTWARE OR FOR ABB SERVICES COMPRISED OF DATA, INFORMATION, ANALYSES, ESTIMATES OUTPUT OR MODELS (COLLECTIVELY "INFORMATION"), SUCH INFORMATION IS BASED UPON CUSTOMER'S DATA. CUSTOMER FURTHER ACKNOWLEDGES THAT ABB MAKES NO WARRANTY WITH RESPECT TO SUCH INFORMATION, AND CUSTOMER SHALL NOT RELY ON ABB FOR THE ACCURACY OR COMPLETENESS OF INFORMATION SUPPLIED THROUGH SUCH SOFTWARE OR SERVICES. CUSTOMER ACCEPTS ALL SUCH INFORMATION ON AN "AS IS" "AS AVAILABLE" BASIS.