@charset "UTF-8";

/* SpryValidationCheckbox.css - Revision: Spry Preview Release 1.4 */

/* Copyright (c) 2006. Adobe Systems Incorporated. All rights reserved. */


/* These are the classes applied on the messages
 * (required message, minSelections message and maxSelections message)
 * which prevent them from being displayed by default.
 */
.checkboxRequiredMsg, .checkboxMinSelectionsMsg, .checkboxMaxSelectionsMsg{
	display: none;
}

/* These selectors change the way messages look when the widget is in one of the error states.
 * These classes set a default red border and font color for the error text.
 * The state class (e.g. .checkboxRequiredState) is applied on the top-level container for the widget, 
 * and this way only the specific error message can be shown by setting the display property to "inline".
 */
.checkboxRequiredState .checkboxRequiredMsg,
.checkboxMinSelectionsState .checkboxMinSelectionsMsg,
.checkboxMaxSelectionsState .checkboxMaxSelectionsMsg {
	display: inline;
	color: #CC3333;
	border: 1px solid #CC3333;
	margin: 0px;
	padding: 1px 3px;
	height: 1px;
}