Looking for old site? Looking for old site?

Looking for our old site?

We officially launched our new site on March 8, 2015.  There are many new features and we trust you’ll like the new site once you have a chance to explore all it can offer you.

While we hope our old sites served you well, unfortunately they are showing their age and we will be retiring them soon.  However, if you’re in a super big hurry and don’t have time to learn the new site, you can get to the old sites below for a limited time.

Old Sites
 www.baldor.com www.dodgept.com
 www.reliance.com www.dodge-reliance.com
Go
  • Quantis Build Center in Dallas

    Big things happen in Dallas… like the new Baldor•Dodge Quantis® Build Center. Baldor’s Dodge Quantis Build Center in Dallas, TX can now assemble Quantis In-Line (ILH) gear reducers as well as Motorized Shaft Mount (MSM) gear reducers and screw conveyor drives.
  • Webinar - Shaft Grounding and Current Mitigation

    Are you using variable frequency drives (VFD) for optimum efficiency in your application? Join us May 27th for a live webinar as we team up with Plant Services magazine to discuss the importance of protecting your motor when it’s controlled by a VFD.
  • ON-DEMAND WEBINAR: Impact of the Integral Horsepower Rule (1 – 500 HP motors)

    The National Electrical Manufacturers Association (NEMA) and a coalition of energy advocates submitted a petition to the Department of Energy to increase efficiency in industrial electric motors not covered under the latest small motor rule.
  • Baldor's G-Series Above NEMA Vertical P-Base Motors

    Baldor Electric Company is proud to announce the Above NEMA Vertical P-Base Motor platform.
  • ABB - Solid Growth in a Mixed Market

    “We delivered a solid first quarter in which we grew net income and increased cash flow, in line with our commitment to drive profitable growth and accelerate sustainable value creation,” said CEO Ulrich Spiesshofer.
  • Baldor Electric Honored with United Way 2014 Chairman’s Award

    The Baldor Electric facilities in the Fort Smith, Arkansas area were honored this week to receive the United Way of Fort Smith Area 2014 Chairman’s Award. This award goes to a company that continually demonstrates dedication and commitment to United Way. Baldor was recognized for employee giving and being a loyal partner to the 34 local agencies.
  • Visit Baldor at the Offshore Technology Conference 2015

    Are you attending the 2015 Offshore Technology Conference, May 4 – 7 in Houston? If so, make sure that you visit us in Booth #5740 to see how we can help you find solutions to your projects in the oil and gas industries.
  • Find Us at Coal Prep 2015

    Are you attending Coal Prep 2015 in Lexington, KY this year? If so, be sure to visit Baldor Electric at Booth #1605 to see how we can help you with your coal preparation and processing. Featured in the Baldor booth will be a right angle MagnaGear G285 hollow shaft reducer that uses the patented Dodge twin tapered bushing mounting system for ease of installation and removal.
  • Quantis Build Center in Dallas

    Big things happen in Dallas… like the new Baldor•Dodge Quantis® Build Center. Baldor’s Dodge Quantis Build Center in Dallas, TX can now assemble Quantis In-Line (ILH) gear reducers as well as Motorized Shaft Mount (MSM) gear reducers and screw conveyor drives.
  • ABB - Solid Growth in a Mixed Market

    “We delivered a solid first quarter in which we grew net income and increased cash flow, in line with our commitment to drive profitable growth and accelerate sustainable value creation,” said CEO Ulrich Spiesshofer.
  • Baldor Electric Honored with United Way 2014 Chairman’s Award

    The Baldor Electric facilities in the Fort Smith, Arkansas area were honored this week to receive the United Way of Fort Smith Area 2014 Chairman’s Award. This award goes to a company that continually demonstrates dedication and commitment to United Way. Baldor was recognized for employee giving and being a loyal partner to the 34 local agencies.
  • Visit Baldor at the Offshore Technology Conference 2015

    Are you attending the 2015 Offshore Technology Conference, May 4 – 7 in Houston? If so, make sure that you visit us in Booth #5740 to see how we can help you find solutions to your projects in the oil and gas industries.
  • Find Us at Coal Prep 2015

    Are you attending Coal Prep 2015 in Lexington, KY this year? If so, be sure to visit Baldor Electric at Booth #1605 to see how we can help you with your coal preparation and processing. Featured in the Baldor booth will be a right angle MagnaGear G285 hollow shaft reducer that uses the patented Dodge twin tapered bushing mounting system for ease of installation and removal.
  • Webinar: How Gearmotor Technology Increases Vertical Pump Drive Efficiency

    In today’s high-volume pumping applications, energy efficiency and cost control are more important than ever. A new solution using low-pole-count induction motors and proven gear motor technology offers effective results to these important challenges.
  • Baldor Electric Launches New Website with Powerful Search & Download Capabilities

    Baldor Electric Company is excited to announce the new Baldor.com website, a robust destination site for North American industrial motor and mechanical users.
  • Baldor Electric Executive Recognized for Excellence in Manufacturing

    The Manufacturing Institute has announced it will award Amy Lakin, executive vice president of Supply Chain for Baldor Electric Company, with the Women in Manufacturing STEP (Science, Technology, Engineering and Production) Ahead Award.
  • Baldor's G-Series Above NEMA Vertical P-Base Motors

    Baldor Electric Company is proud to announce the Above NEMA Vertical P-Base Motor platform.
  • New Baldor•Dodge Type EXL Four-Bolt Flange Tapered Roller Bearing

    Baldor Electric is proud to announce a new addition to our tapered roller bearing family, the Baldor•Dodge Type EXL four-bolt flange bearing. Type EXL flange bearings provide superior sealing, misalignment and expansion capability as well as the highest load ratings in the industry.
  • Baldor Is Proud to Offer ABB's Expanded Line of New Rib-Cooled Motors

    Baldor Electric Company is proud to offer ABB’s expanded line of high voltage rib-cooled motor platform, type NXR, with higher power ranges and increased ingress protection.
  • Baldor Introduces the Baldor•Dodge Vertical Gearmotor

    Baldor Electric announces a new addition to our gear reducer product offering, the Baldor•Dodge Vertical Gearmotor. The Vertical Gearmotor offers a cost effective alternative to the common low speed vertical pump drive technologies, which utilize large, high pole count vertical motors or a combination of horizontal motor with a right angle gear reducer.
  • New Baldor•Reliance Crusher Duty Motors: Enhanced Line in the Severe Duty Family

    Baldor Electric Company introduces a new line of crusher duty motors with improved reliability, performance, and energy efficiency to help lower the operator’s total cost of ownership. With higher break down and locked rotor torque performance, Baldor●Reliance® crusher duty motors meet the demands of the toughest crushing applications worldwid
  • Baldor•Dodge Ultra Kleen Tigear-2: The Newest Addition to Baldors Washdown Family

    Baldor Electric Company is proud to announce a new addition to our washdown family of enclosed gear reducer products, the Baldor•Dodge Ultra Kleen® Tigear-2®.
  • New Offering from Baldor-Dodge: Disc Coupling ATEX Certification

    Baldor Electric is proud to provide ATEX certification for all Baldor-Dodge Disc Couplings. ATEX is a European Union directive which defines essential health and safety requirements for all equipment used in potentially explosive atmospheres. The Disc Coupling meets all ATEX requirements for mining applications and other applications with combustible dust and gas atmospheres.
  • The New Dodge QD Para-Flex Coupling

    Baldor Electric is proud to announce a new addition to our Baldor-Dodge coupling product offering: The QD Bushed Para-Flex® coupling. To complement our Taper-Lock and bored-to-size style flanges, the QD flange design now enhances our industry leading capabilities.
  • Webinar - Shaft Grounding and Current Mitigation

    Are you using variable frequency drives (VFD) for optimum efficiency in your application? Join us May 27th for a live webinar as we team up with Plant Services magazine to discuss the importance of protecting your motor when it’s controlled by a VFD.
  • ON-DEMAND WEBINAR: Impact of the Integral Horsepower Rule (1 – 500 HP motors)

    The National Electrical Manufacturers Association (NEMA) and a coalition of energy advocates submitted a petition to the Department of Energy to increase efficiency in industrial electric motors not covered under the latest small motor rule.
  • Manufacturers Hope to Enlist Young Adults

    Tough. Dirty. Low-paying. Those are just a few of the things. Arielle Holland had in mind when she first considered taking a job at Baldor Electric Company, a manufacturer with a plant in Flowery Branch.
  • Why Do Motor Drives Impact the World so Dramatically?

    Motor drives, which act exactly like an accelerator pedal that speeds up or slows down a vehicle in exact proportion to driving conditions, are the unsung heroes of the energy world.
  • Washdown Pump Motors Provide Reliable Sanitary Operation

    When thinking of a food manufacturing facility, many people may envision a lockdown area in which all personnel must wear full-body decontamination suits and where every internal surface of the facility must glow from the sheen of stainless steel. While this may be somewhat common for parts of a plant, a range of environments allow for different grades of motors, from general purpose to washdown, which drive many pumping applications.
  • Webinar: The Impact of the Integral Horsepower Rule (1 - 500 HP motors)

    The National Electrical Manufacturers Association (NEMA) and a coalition of energy advocates submitted a petition to the Department of Energy to increase efficiency in industrial electric motors not covered under the latest small motor rule. A Final Rule was issued in March, 2014 which will broaden the scope of coverage left behind from the Energy Independence & Security Act (EISA) of 2007. The Integral Horsepower Rule will go into effect June 1, 2016 and supersede the EISA 2007 laws.
  • Webinar: Improving Reliability and Productivity in Harsh Sanitation Environments

    Over the past few years, a common practice in the Food and Beverage Industry is to evaluate system components to improve reliability, productivity and food safety in harsh sanitation environments. Washdown motors and bearings are just two products where selecting the right feature set provides extended life and better performance in the harsh environments typical to the industry.
  • Will the Small Motor Rule Affect You?

    Mark your calendar for March 9, 2015. The United States Department of Energy issued a Final Rule in March of 2010 mandating energy efficiency levels be increased – effective March 9, 2015. The rule affects a very specific range of motors which include NEMA two-digit frame motors and IEC equivalents for Open Drip Proof, General Purpose motors in both single and three phase designs.

Recent Tweets

Recent Videos